AXIS#.CMDSOURCE

Description

AXIS#.CMDSOURCE specifies the source of the command to the axis. AXIS#.OPMODE sets the operation mode to the relevant control loop.

AXIS#.CMDSOURCE values can be set as follows:

Value

Description

0

Service, TCP/IP command

1

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design command

2

Gearing command

3

Analog command

4

Gantry Mode


  • Only available on Axis 2

AXIS#.CMDSOURCE can be changed while the drive is enabled or disabled. If using the terminal to change the operation mode, it is recommended to disable the drive before changing the command source.


  • If you change AXIS#.CMDSOURCE from the terminal while the drive is enabled, the system may experience a step change in command.

Example

To set the command source to the TCP/IP channel and the operation mode to velocity:

-->CMDSOURCE 0

-->OPMODE 1

Versions

Action Version Notes
Implemented 02-00-00-000
Value 4 added 02-02-05-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 4

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.CMDSOURCE

5000h

0eh

Unsigned8

-

-

Read/Write

No

AXIS2.CMDSOURCE

5100h

0eh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.CMDSOURCE

5004

138C

Unsigned8

Read/Write

-

AXIS2.CMDSOURCE

70540

1138

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.CMDSOURCE

5004

Unsigned8

Read/Write

-

Related Topics

AXIS#.OPMODE

Gantry Mode